KANSAS CITY, Missouri – Labconco Unveils Second TUV EN 12469 Certified Microbiological Safety Cabinet
Labconco® is excited to release the ReVo™, another innovative microbiological safety cabinet, adding to its diverse biosafety portfolio. The ReVo is a new Class II, Type A2 solution for biosafety, thoughtfully designed with simplicity in mind.
The ReVo provides personnel, product and environmental protection from hazardous pathogens and particles with multiple features that enhance performance and containment. Advanced blower technology with CAP™ constant monitoring creates a quiet, sterile working area to protect users and their samples. A comprehensive user interface notifies users of unsafe conditions through clear visual and audible signals. Each model includes a full stainless-steel interior for easy cleaning and decontamination, and cabinet construction is approved by TUV Nord to the EN 12469 standard.

ReVo safety cabinets offer unsurpassed comfort through ergonomic design, including inflow grilles angled to provide comfortable posture, a glare-free 270-degree panoramic view of the work space, and conveniently positioned display and controls. It’s also one of the quietest MSCs in the world. Laboratories can conduct their research in a low-noise working environment, even when multiple MSCs are positioned in the same room.
Labconco products excel at reducing the energy burden of their equipment without compromising performance, and the ReVo exemplifies that commitment. It offers extreme energy efficiency, plus Night-Smart™ technology that intelligently reduces blower speed between uses to save energy while maintaining a sterile environment.
Labconco's Director of Biosafety Products, David Wasescha, said of the announcement, "The ReVo is the result of our ongoing dialogue with life science laboratories all over Europe and beyond. It is another step in our commitment to provide advanced biosafety containment tools to all forms of researchers in the high-growth life science market."
Labconco is a global leader in biosafety products with over 50 years of experience, and a leading manufacturer of scientific and healthcare engineering control devices for nearly 100 years. At the forefront of innovation worldwide, Labconco continues to provide tested and true solutions for all ranges of biosafety.
To find out more about the ReVo, contact Labconco or visit labconco.com/revo.
VIEW AND SHARE ONLINE
About Labconco
Labconco enhances global scientific discovery by providing exceptional equipment and service. Serving the scientific community since 1925, Labconco Corporation manufactures laboratory equipment, specializing in ventilation enclosures such as chemical fume hoods and biological safety cabinets. Labconco also produces glassware washers, freeze dryers, evaporators, glove boxes and specialized forensic enclosures. Labconco equipment can be found in academic, industrial, life science, pharmaceutical, environmental, forensic and clinical laboratories worldwide.