Skip to main content

FAQs

What is a high performance fume hood?

A High Performance fume hood (defined by SEFA 1) is engineered to maintain safe containment at lower airflow volumes than traditional designs. Instead of relying on high face velocity, these hoods optimize aerodynamics to improve containment efficiency. The result is reduced exhaust demand and significant energy savings without compromising safety.

  • Typically operates effectively at 60–80 FPM.

  • Designed to pass SEFA requirements on ASHRAE 110 tests with 60 fpm face velocity at full open sash.

  • Reduces HVAC load and operating costs.

The appropriate fume hood face velocity should be determined by each organization's safety and facilities teams through a documented risk assessment. Face velocity is a safety decision, and the requirements depend on several site-specific factors, including the hazards involved, hood design, room airflow conditions, and operating practices.

While many laboratory fume hoods operate between 80 and 100 feet per minute (fpm), High Performance hoods can provide acceptable protection with velocities as low as 60 fpm, and certain applications may require velocities above 100 fpm. Both excessively high and excessively low face velocities can negatively impact containment performance.

  • Typical fume hood face velocities are often 80-100 fpm, but there is no one-size-fits-all value.

  • High-performance fume hoods may achieve effective containment at 60 fpm when properly designed and validated.

  • Face velocities that are too high can create turbulence, while velocities that are too low may not provide adequate containment.

  • ANSI/ASSP Z9.5 Laboratory Ventilation provides valuable guidance for conducting risk assessments and establishing appropriate face velocity criteria.

This is often asked for fume hoods installed on a variable air volume (VAV) system. For VAV fume hoods, there is no universal minimum airflow requirement when a hood is closed or idle. The appropriate minimum airflow should be determined through a risk assessment that considers factors such as room pressurization, directional airflow, ventilation strategy, potential hazards, and energy-saving objectives. While modern fume hoods can often reduce airflow to very low levels when not in use, the selected minimum is typically driven by overall laboratory requirements rather than the fume hood itself.

  • Minimum airflow should be based on a laboratory-specific risk assessment.

  • Idle airflow settings often support room pressurization and directional airflow goals.

  • Modern VAV fume hoods may be capable of operating at very low airflow rates when closed.

  • Seek guidance from industry standards (such as ANSI/ASSP Z9.5 Laboratory Ventilation) establishing appropriate minimum airflow setpoints.

The right fume hood depends on the specific hazards, chemicals, and processes involved in your application. The first step is evaluating the risks and selecting a hood with materials of construction that are compatible with the substances being used. Once compatibility and safety requirements are established, factors such as hood size, equipment requirements, available laboratory space, and the building's mechanical system can help determine the most appropriate solution.

  • Select a hood with materials compatible with the chemicals and processes involved.

  • Size the hood based on equipment dimensions, work practices, and available space.

  • Consider how the hood will integrate with the laboratory's ventilation and mechanical systems.

  • Use a risk assessment to identify hazards and define the appropriate fume hood requirements.

An explosion proof fume hood is designed for environments where ignitable levels of flammable vapors (or particulate) may be present and ignition sources must be controlled. Importantly, the hood itself does not contain explosions — rather, electrical components are either removed or rated to prevent ignition via spark potential. Proper classification of the lab space determines if EP components are required.

  • All electrical components to be rated for hazardous locations.

  • Required in locations with a hazardous classification (NFPA 70).

  • Not designed to contain an explosion.

  • Should align with local fire marshal guidance.

Industry standards recommend that fume hoods be certified annually to verify that they are operating safely and providing adequate containment. Certification requirements may vary by organization, but laboratories should follow the policies established by their facility's safety team and applicable regulatory requirements. Fume hoods should not be used if they are out of certification or if their performance has not been verified.

  • Annual certification is the recommended industry practice.

  • Comprehensive performance verification may include face velocity testing, smoke visualization, and ASHRAE 110 containment testing.

  • Certification requirements should be established by the facility's safety and environmental health teams.

  • Do not use a fume hood that is overdue for certification or has failed performance testing.

In general, fume hoods are safest when they remain operating continuously, as constant exhaust helps maintain negative pressure and provides protection if hazardous materials, residual contamination, or unexpected releases remain in the hood. However, some facilities choose to turn fume hoods off for operational or energy-saving reasons. When this occurs, the hood should be properly decontaminated, safeguards should be in place to prevent backdrafting, and the impact on overall laboratory ventilation must be carefully evaluated.

  • Leaving a fume hood on continuously is generally the preferred safety practice.

  • Hoods that are turned off should be decontaminated before shutdown.

  • Backdraft prevention measures should be implemented when exhaust is not operating.

  • Consider the effect on room pressurization and directional airflow before shutting down a hood.

Ductless fume hoods provide containment in a manner similar to traditional ducted fume hoods by drawing air through the hood opening and away from the user. The key difference is that, instead of exhausting air outside the building, a ductless hood passes contaminated air through specialized filtration media, typically activated carbon. Hazardous vapors are adsorbed onto the filter media, and the filtered air is then recirculated back into the laboratory. Because filtration performance depends on the chemicals being used, a chemical assessment should be completed before selecting a ductless fume hood to verify compatibility and expected filter life.

  • Ductless hoods filter and recirculate air rather than exhausting it outdoors.

  • Activated carbon filters remove many chemical vapors through adsorption.

  • A chemical assessment should be completed to verify chemical compatibility and filter service life.

  • A breakthrough or saturation alarm should be present to provide users with real-time alerts when the carbon media is loaded, and filters need to be replaced.

The suitability of a ductless fume hood must be determined through a chemical assessment completed by the facility and reviewed by the hood manufacturer. This assessment evaluates the chemicals, quantities, processes, and operating conditions to determine whether the application can be safely supported by filtration technology. If approved, the manufacturer can provide guidance on filters and estimated life expectancy. If the application is not suitable for a ductless fume hood, a ducted fume hood will generally be required.

  • Complete a chemical assessment for each application before selecting a ductless fume hood.

  • The manufacturer reviews the assessment and provides approval or recommendations.

  • Approved applications typically include expected filter life.

  • If the application cannot be safely filtered, a ducted fume hood should be used instead.

While fume hoods and biological safety cabinets (BSCs) may look similar, they are designed to protect against different hazards. A fume hood provides personnel protection from hazardous chemical vapors, gases, and fumes by exhausting contaminated air away from the user. A BSC is designed to provide both personnel protection and product protection by controlling airflow and filtering air through HEPA filters to contain biological agents and particulate contaminants.

Selecting the correct equipment is critical. Using a BSC for chemical vapor hazards or a fume hood for work requiring product sterility can compromise safety, contaminate processes, and increase the risk of exposure.

  • Fume hoods protect personnel from hazardous chemical vapors, gases, and fumes.

  • BSCs protect both personnel and products from biological agents and particulate contaminants.

  • Fume hoods and BSCs use different airflow patterns, filtration methods, and materials of construction to support their intended applications.

  • Choosing the wrong device can result in inadequate protection, product contamination, or personnel exposure.

The primary difference between constant air volume (CAV) and variable air volume (VAV) fume hoods is what remains constant as the sash position changes. A CAV fume hood maintains a constant exhaust airflow rate, which means the face velocity increases when the sash is closed and decreases when the sash is opened. A VAV fume hood adjusts the exhaust airflow rate to maintain a more consistent face velocity as the sash moves. When properly designed, VAV systems can help improve safety, maintain desired airflow conditions, and reduce energy consumption by lowering exhaust volumes when hoods are not in use.

  • CAV hoods maintain a constant exhaust volume, causing face velocity to vary with sash position.

  • VAV hoods vary exhaust volume to maintain a more consistent face velocity with changing sash positions.

  • CAV systems are generally simpler and lower cost than VAV systems.

  • VAV systems can provide energy savings and advanced ventilation control through integration with the building HVAC system.

The life expectancy of a fume hood depends heavily on the application, frequency of use, chemical exposure, and maintenance practices. A properly selected fume hood that is routinely cleaned, maintained, and used within its design limits can often remain in service for 20 years or more. However, exposure to incompatible chemicals, poor maintenance, or demanding operating conditions can significantly reduce its useful life.

While every installation is different, many facilities can reasonably expect a well-maintained fume hood to provide 15 to 20 years of service before replacement is required.

  • Properly selected and maintained fume hoods can often last 20+ years.

  • Typical service life for most laboratory environments is 15-20 years.

  • Chemical compatibility, usage, and operating conditions greatly influence longevity.

  • Regular cleaning, inspection, and maintenance can help maximize fume hood life expectancy.