HomeLab & Science NewsArticlesVideo: Creation Story of the Axiom Type C1 Biosafety Cabinet

Video: Creation Story of the Axiom Type C1 Biosafety Cabinet

Scott Anthony PattersonBy Scott Anthony Patterson, Marketing Content Manager
On Tuesday, July 25, 2017
In Articles

The Purifier Axiom Type C biosafety cabinet replaces Type A2 and Type B2 biological safety cabinetsBrian Garrett feels a deep obligation to provide biosafety equipment that is "as bullet proof as possible" for the protection of the scientists and researchers on the front lines. Every day they make new discoveries and defend us against new risks, new agents and threats to our health. 
 
Garrett and his team of engineers at Labconco developed the Type C1 to eliminate the need for all other types of biological safety cabinets. They combined features of type A2 and type B2 cabinets in a way that most in their field had thought impossible, to create a safer, more reliable, more useful work space.
 
Laboratory building design, life science lab work flow and lab safety all took a giant leap forward from decades old Type A2 and Type B2 technology with the creation of this new type of Class II biosafety cabinet.
 
 

Find out more about the Purifier Axiom

Related Product Categories
Type C1 Axiom biosafety cabinet, class II biosafe cabinet

Biological Safety Cabinets & Enclosures

Class I and Class II biological safety cabinets are suitable for use with agents that require Biosafety Level 1, 2 or 3 containment.

See Details

Logic+ A2 with model 800

Class II, Type A2 Biosafety Cabinets

These cabinets protect the user, product and lab. They recirculate 70% of the HEPA-filtered laminar air while 30% passes through an exhaust HEPA filter for discharge to the lab or optional canopy.

See Details

Cell Logic Plus B2 Scope-Ready with model 800

Class II, Type B2 (Total Exhaust) Biosafety Cabinets

These total exhaust cabinets protect the user, product and lab. They are designed to be hard ducted to the outside, exhausting 100% of the HEPA-filtered air outside the lab.

See Details

Axiom with R&D 100 2016 Awards Finalist Logo and model

Class II, Type C1 Biosafety Cabinets

The first BSC with the flexibility to convert from A2 to B2 mode. Simple to use, with unmatched chemical safety.

See Details