HomeLab & Science NewsArticlesThe good, the bad and the ugly of UV light usage in a Class II BSC

The good, the bad and the ugly of UV light usage in a Class II BSC

Brian Garrett 2013By Brian Garrett, LEED Green Associate, Product Manager
On Tuesday, August 16, 2016
In Articles

For decades, germicidal UV lamps have been used in Class II Biological Safety Cabinets. The purpose is to keep a biosafety cabinet’s interior clean when not in use. Many researchers swear by the use of their UV lamp and would never consider owning or buying an enclosure without one. Others believe UV lamps provide a false sense of security or don’t see the merit in a UV lamp (such as the NIH). Germicidal lamps utilize UVc radiation (typically at 254 nm wavelength). This energy is very good at doing a specific task, but it’s a poor broad spectrum decontaminant, and here is why:

The Good:UVc is a recommended accessory for your BSC or laminar flow bench when working with cell cultures, PCR or other genetic materials because UVc radiation is efficient at breaking up chemical bonds and denaturing DNA and RNA. Under prolonged exposure, these chemical changes lead to dysfunctional genetic material and eventual cell death.

The Bad: Germicidal lamps use low energy radiation—so low that the waves are incapable of penetrating barriers or of reflecting from most surfaces. This simply means that for UV lamps to be effective, the target MUST be in direct line of sight with the light source. This is bad if you are using a germicidal lamp as the primary decontaminant in your lab’s culture enclosure. However, for those folks populating the lab or standing outside of the enclosure with nothing but a sheet of glass between them and the blue tube of light, this is a good thing. It means that sheet of glass is more than sufficient to block you from becoming irradiated.

The Ugly: Use of a UV lamp for the purpose of primary decontamination is rampant, as is the frequency of cross contamination. True, cross contamination can be caused by a number of factors – but experience shows that labs utilizing UV lamps as the only means of “cleaning” their BSC have a higher prevalence of such issues.

Two simple rules for using UV lamps

1.     If you are using “naked” DNA / RNA or performing PCR... UV lamps are excellent at rendering these materials harmless.

2.     If you are doing anything else with biological material… do not rely on UV lamps alone to keep your work area clean. ALWAYS wipe down exposed surfaces with a proper decontaminant PRIOR to turning on the UV lamp. ALWAYS wipe down exposed surfaces with a proper decontamination AFTER turning off the UV lamp.


Learn about the new Type C1 biosafety cabinet. It does the work of an A2 and a B2 at a lower cost of ownership.

Related Product Categories
Axiom without duct, no model 1200

Biological Safety Cabinets & Enclosures

Class I and Class II biological safety cabinets are suitable for use with agents that require Biosafety Level 1, 2 or 3 containment.

See Details

Filtered PCR Enclosure with model

PCR Enclosures

These enclosures are specially designed for use with polymerase chain reaction experiments.

See Details