|| || Product Literature >> Centrifugal Concentrators & Cold Traps >> Developing a Vacuum Concentration Protocol

Developing a Vacuum Concentration Protocol

Efficient removal of solvents by vacuum concentration is a routine step for many analytical and isolation protocols. For the most part, protocols simply involve spinning the sample while applying a vacuum. The vacuum concentrator reduces the atmospheric pressure which in turn lowers the boiling point of the solution. The centrifugal force keeps the sample from boiling out of the tube, which is a phenomenon generally referred to as "bumping." However, some solutes are negatively affected by both temperature and solute concentration changes that occur during processing. For optimum yield and preservation of biological activity (when applicable), these parameters should be considered for each new solute and solvent combination.

Solute Properties and Guidelines for Concentration

The ease by which a solute can be concentrated is dependent upon the characteristics of the solute and solvent. A rugged molecule, such as DNA, is easily concentrated when in aqueous solution. It can be heated and concentrated to dryness and will still function properly when introduced into a cell. The characteristics of the solvent being vaporized have a major impact on the process as well. Volatile solvents are much easier to remove. However, the ease by which solvent is removed from a sample is secondary when compared to the resulting quality of the concentrated solute product.

Not all solutes have the fortitude of DNA. Many molecules can be denatured if heated or cooled and may become insoluble if dried. It is therefore important to know the limitations of your solute. The following general guidelines can be applied:

When first working with a new molecule, it is difficult to know which parameters affect the solute being concentrated. The best advice is to proceed cautiously until data suggests the degree of abuse your sample can tolerate. This is especially true for proteins.

SmaI

As previously noted, DNA is a rugged molecule easily concentrated to dryness. Unfortunately, many other molecules aren’t as forgiving. For instance, restriction enzyme, SmaI, is very sensitive to changes in temperature. It is inactivated by both heat (> 65°C) and extreme cold.

SmaI was diluted to a concentration of 1 U/μl in water and concentrated using a CentriVap vacuum concentrator by three methods. The enzyme was then re-hydrated in 1X restriction enzyme buffer and tested for activity by cleaving λ DNA. Concentrating the enzyme to the point of dryness at room temperature using low vacuum has little effect on the SmaI activity. Using high vacuum conditions causes a solution of the enzyme to concentrate by freeze drying, which has little effect on enzyme activity. However, concentrating the enzyme using high vacuum but without freezing the solution results in loss of activity. Results are summarized in Figure 1.

Figure 1. The fate of SmaI is unexpected when vacuum concentrated. Lane 1 is a SmaI control used to digest λ DNA at 25°C. Lane 2 represents enzyme dried under low vacuum, and lane 3 was freeze dried under high vacuum with sufficient heat removal to freeze the sample. The SmaI of lane 4 was concentrated under low vacuum at 4°C. All lanes exhibit activity except lane 4.

Effect of High Salt Concentration

Other proteins are tolerant of high and low temperatures, but may become inactive or insoluble in high salt concentrations. The dehydration and inactivation of proteins during freeze drying can be caused by local accumulation of salt ions. One method used to reduce the concentration of salt ions prior to solute concentration is buffer exchange. Gel filtration with G10 or G15 Sephadex (GE Healthcare, Piscataway, NJ) can be used to exchange buffers on peptides, proteins and other high molecular weight solutes. Generally samples become more dilute after gel filtration, but the water will soon be removed during concentration.

Result Between Surface Area, Temperature, and Pressure

The parameters that affect solutes during vacuum concentration are not limited to temperature. The interrelationship between surface area, temperature, and pressure also affects sample integrity. When a vacuum is applied, the sample temperature will decrease as solvent molecules vaporize. In a process referred to as adiabatic expansion, internal energy of the sample is transferred as solute moves between phases. As the vacuum removes the solvent vapors, the temperature of the liquid decreases and the rate of vaporization (or sublimation if the sample is frozen) slows. With room temperature water (500 μl in a microcentrigure tube), the sample temperature can decrease to -25°C in just a few minutes after applying a high efficiency vacuum (Figure 2). Methanol, which is more volatile than water, drops to below -40°C under the same conditions. It is also important to note that methanol boils at 64.7°C. Figure 3 demonstrates these differences.

Vacuum concentrators process solute and solvent and yield solute concentration

Figure 2. The temperature of water decreases rapidly when a deep vacuum is applied. As water molecules vaporize, heat is removed from the system which eventually leads to freezing. The rate of water loss then slows as the heat required for sublimation is greater than vaporization.

Figure 3. Vaporization of methanol and water demonstrates the nature of solvent volatility on concentration. Methanol was completely vaporized in approximately half the time of water. The methanol/ water mixture shows a hybrid vaporization pattern.

Impact of Solvent Properties on the Concentration Process

The difference in vaporization between methanol and water illustrates the importance of solvent properties on the concentration process (Table 1). In comparing these solvents, the key property that affects concentration is boiling point. As vacuum is applied to the solvents and the boiling point decreases, molecules readily vaporize. Consequently, the order of solvent evaporation rate during sample concentration is methanol> ethanol > water (Figure 4).

Table 1. Physical properties of common solvents.

Solvent

Melting/Freezing Point

Boiling Point

Water

0.0

100.0

Ethanol

-114.1

78.5

Methanol

-97.7

64.7

Figure 4. The graph illustrating the concurrent evaporation of methanol, ethanol, and water samples in a CentriVap Centrifugal Concentrator demonstrates that solvents with lower boiling points vaporize most rapidly. This processing represents 500 μl of solvent evaporated with a high efficiency vacuum pump for 1 hour.

Effect of Freezing Point on Concentration

Solvent freezing point also affects the concentration process, a factor very apparent when water is the solvent. Under high efficiency vacuum conditions, water vaporizes until it freezes. At that point, water loss is through sublimation, which requires greater heat energy than vaporization. A comparison of the rate of vaporization from water and phosphate buffered saline demonstrates this point (Figure 5). Using a CentriVap Centrifugal Concentrator with a high efficiency vacuum pump, water freezes more rapidly than the phosphate buffered saline due to the presence of salt in the latter. Though the PBS does eventually freeze the small time lag results in greater water loss from the PBS samples.

Figure 5. Vaporization of water and phosphate buffered saline (PBS) demonstrates that liquid samples vaporize at a rate faster than frozen samples. Logically, more energy is required to change in phase from solid to gas than from liquid to gas.

Introduction of Heat

Many vacuum concentrators introduce heat into samples to enhance vaporization. Although this can be effective, it is very dependent upon the type of system employed. Commercial centrifugal concentrators, such as the CentriVap, can provide temperature control to the chamber. Most models can heat, but the CentriVap is also available with built-in refrigeration (a useful feature for temperature sensitive proteins and analytes). However, an adjustment of atmospheric pressure may be necessary for heated chambers to be effective at accelerating vaporization.

Introducing heat into samples during the concentration process will not necessarily increase the temperature of the sample. If the atmosphere in the concentrator is under a near full vacuum, then heat introduced by the chamber walls will not affect the sample. Convection works by increasing the temperature (molecular motion) of the gas molecules in the local atmosphere. If there is little or no atmospheric pressure, which corresponds to a reduced number of atmospheric gas molecules, then heat transfer is ineffective. Using a bleed valve or lower efficiency vacuum pump will increase the level of atmosphere pressure in the concentrator so that chamber heat is transferred to the sample. At high pressure, aqueous samples are less likely to freeze as well. This is especially important when concentrating bioactive compounds such a protein.

Phase Effect on Concentration

A comparison of sample water loss using CentriVap under high vacuum, high vacuum with infrared light, and low vacuum demonstrates the phase effect on the concentration process (Figure 6). The high efficiency vacuum is most effective at vaporizing water when the sample is liquid and the starting temperature is high. However, as the sample cools and freezes, the rate of water loss slows. Introducing heat by infrared radiation further enhances vaporization, but as the sample cools and eventually freezes, the rate declines again. Although low vacuum pressure is though initially slow, the results are similar to those using a high efficiency vacuum. Though initial water loss is less, the rate eventually becomes greater since the sample does not freeze.

Figure 6. Comparison of water loss using high vacuum and low vacuum. Low vacuum concentration, though initially lagging, surpassed high vacuum concentration as the sample remained liquid.

Effect of Surface Area on Concentration

The surface area of the liquid also affects the rate of solvent loss. By increasing the surface area, solvent more readily escapes from solution. This implies that solvent contained in long, thin tubes or vessels will vaporize slower than with shorter containers with wider openings. Tubes placed in a vacuum concentrator rotor at an angle will have a slanted surface area while spinning, a simple but effective trick for improving concentration.

Summary

In order to effectively concentrate a solute, several important factors must be considered. Foremost, the parameters that allow for solute stability must be identified and built into the process. High salt content, over drying, and extreme temperatures (both high and low) can all negatively affect solute integrity. Simply put, the concentration protocol must maintain parameters suitable to maintain stability for the solute being concentrated. If a choice of solvent is possible, using the solvent with the lower boiling point will result in faster evaporation. Also use a vacuum level that is appropriate for your solute being concentrated. High efficiency vacuum may speed concentration, but loss of heat may cause the solvent to freeze and slow the process. Finally, use a large surface area to speed the removal of solvent from the sample.

. (Login Required)