HomeLab & Science NewsArticlesMaking a better chocolate, whiskey-style (part 3 of 3)

Making a better chocolate, whiskey-style (part 3 of 3)

Jessica BurdgBy Jessica Burdg, Science Journalist
On Monday, January 12, 2015
In Articles

PREVEIOUS: Making a better chocolate, whiskey-style (part 2 of 3)

The end result, though, is worth it: a powder that world-renowned chocolatier Christopher Elbow will use to create a one-of-a-kind delicacy.

"When it gets to me, it's a simple matter of melting and tempering the bar, then adding the freeze dried whiskey," Elbow says.

An appreciation for the uniqueness of this project is shared by all involved, especially in the Labconco lab where the freeze-drying occurs.

THE NEXT STEP

All parties agree that this process—flavor extraction and infusion into substances like chocolate—is an evolving one. The technique is reproducible, as they've also been able to lyophilize fresh strawberries for infusion into ice cream. Like most things worth doing, though, using lyophilization to isolate flavors is not without its challenges.

Currently, the experts at Labconco are working on increasing yield while maintaining the aromatic profiles of the final product.

"The whole process has been trial and error," Goldstein says. "Now, we are trying to get a larger quantity of the powder while matching the spectra [chemical makeup] of each batch like fingerprints."

Freeze-drying whiskey flavor takes both special equipment and manpower, Prater says, which can make cost-effectiveness a challenge as well.

"From a liter of liquid, we're getting a tablespoon(ish) of the flavor returned in powder form," he says. "Now, it is true that a little goes a long way, but the next step is figuring out how we can make this economical as well. There are a lot of applications."

Elbow says he is happy with the progress of the project and optimistic about the possibilities.

"Now that we have been successful, the challenge is scalability," Elbow says. "We think this is something that could be a pretty niche market."

The one chocolate bar he had so far, though, is enough to keep him going. Elbow, who likes his whiskey on the rocks or in a well-made cocktail, chuckled when asked if that whiskey-flavored chocolate bar was any good.

"Oh yeah," he said. "It was worth it."

To taste some delicious chocolate in person, get a personal glimpse of the extraction technique, and to improve your own lyophilization process development skills, attend the one-time-only class that resulted from this process, a very special Pittcon Short Course in New Orleans.

Related Product Categories
Freeze Dryers

Freeze Dryers

FreeZone Freeze Dry Systems are designed to handle the lyophilization needs of research and pilot plant laboratories. Benchtop and mobile console models are offered, with collectors that reach as low as -105°C.

See Details

Dry Evaporators, Concentrators & Cold Traps

Dry Evaporators, Concentrators & Cold Traps

Labconco dry block evaporators and vacuum concentrators provide sample preparation solutions for a variety of applications.

See Details