HomeLab & Science NewsArticlesLaminar flow in the laboratory: What you need to know

Laminar flow in the laboratory: What you need to know

Jessica BurdgBy Jessica Burdg, Science Journalist
On Thursday, September 08, 2016
In Articles

What is laminar flow?

Laminar flow in the Type C1 in A-Mode and B-Mode

Laminar flow is defined as airflow in which the entire body of air within a designated space is uniform in both velocity and direction.

According to the CDC, the laminar flow principle was first developed in the early 1960s. It's still incredibly relevant for modern labs, having literally shaped the way air safely moves in many generations of laboratory enclosures. Today, many categories of laminar flow hoods exist. Although they differ depending on the science performed within, there is one common denominator: all use this type of unidirectional airflow to aid in maintaining sterility, preventing cross-contamination and reducing turbulence.

Just what exactly is laminar flow, why is it effective and what does it look like in labs today? Let's explore.

How is laminar flow utilized in different types of equipment?

Class II Biosafety Cabinets, sometimes referred to as laminar flow hoods, maintain product protection through HEPA-filtered laminar downflow over the work zone. Per the NSF definition, these ventilated cabinets also feature inward airflow at the open front to protect operators and HEPA filtered exhaust air for environmental protection. 

Class II, Type A cabinets recirculate air back into the laboratory unless a canopy connection is warranted. Class II, Type B cabinets are hard-ducted to the outside. Class II, Type C1 cabinets can function in either Type A or Type B mode. Whichever model suits your application, safe operation within biological safety cabinets is imperative to protect the integrity of your work and your personal safety.

PCR stations, enclosures that are specifically designed to house polymerase chain reaction experiment, utilize the vertical laminar flow of HEPA-filtered air to maintain a particulate-free work environment. A UV light is necessary to denature genetic material (DNA, RNA, etc.) and provide secondary decontamination.

Clean benches are suitable for applications that require product protection, such as media plate preparation or tissue culture maintenance. Air is drawn in through a prefilter located at the top of the clean bench before being pulled through a HEPA filter.

In a vertical clean bench, laminar air is then projected vertically over the work area. In a horizontal clean bench, laminar air is projected horizontally towards the operator. In both instances, laminar flow provides a particulate-free work area.

(Note that some categories of laboratory equipment, like Class I enclosures with perforated baffles or certain high performance fume hoods, employ laminar-like flow. Watch: Airflow in a Class I Enclosure.)

So, what is zoned airflow?

Zoned airflow is not truly laminar. Zoned airflow is used when equipment cannot achieve all of the protection required of a Class II biosafety cabinet with standard laminar airflow. Each zone, or column, of airflow is defined and has its own range in airspeed. This allows for higher speed barrier air columns to be utilized as an engineering solution to equipment that otherwise would have poor containment or product protection ratings.

How does laminar flow differ from dilution flow?

Dilution flow is not the same as laminar flow. The dilution flow principle is used in equipment such as filtered glove boxes. In these instances, HEPA-filtered air mixes with and dilutes interior airborne contaminants inside the glove box, and those contaminants are removed via a filtered exhaust system. After the contamination source has been sealed, the dilution rate—or air changes per minute—will determine how much time must lapse before materials can be removed from the main chamber.

What is turbulent flow?

While laminar flow helps to reduce turbulence, turbulent flow encourages it by creating unintentional swirls of air that place particles randomly on surfaces within an enclosure. Turbulent flow can be disruptive to work that requires a dust-free environment and can lead to contamination. Obstructions, like items left inside enclosures, can create this unwanted turbulence.

For more information on laminar flow or to see it in action, watch this video demonstration:

Related Product Categories
Axiom with R&D 100 2016 Awards Finalist Logo and model

Biological Safety Cabinets & Enclosures

Class I and Class II biological safety cabinets are suitable for use with agents that require Biosafety Level 1, 2 or 3 containment.

See Details

Logic+ A2 with model 800

Class II, Type A2 Biosafety Cabinets

These cabinets protect the user, product and lab. They recirculate 70% of the HEPA-filtered laminar air while 30% passes through an exhaust HEPA filter for discharge to the lab or optional canopy.

See Details

Cell Logic Plus B2 Scope-Ready with model 800

Class II, Type B2 (Total Exhaust) Biosafety Cabinets

These total exhaust cabinets protect the user, product and lab. They are designed to be hard ducted to the outside, exhausting 100% of the HEPA-filtered air outside the lab.

See Details

Axiom with R&D 100 2016 Awards Finalist Logo and model

Class II, Type C1 Biosafety Cabinets

The first BSC with the flexibility to convert from A2 to B2 mode. Simple to use, with unmatched chemical safety.

See Details