HomeLab & Science NewsScience NewsAdding Efficiency to Labs

Adding Efficiency to Labs

Beth Mettlach 2014By Beth Mankameyer, Sales Engineer
On Thursday, May 05, 2016
In Science News

Energy efficiency in a lab can be worth thousands of dollars of savings per year. Equipment such as a single fume hood can use the equivalent energy of three and a half single family homes per year [1] making energy efficiency a priority for labs.

This article talks about a few things labs can be mindful of in order to keep their bills in check, including a special shout-out to Labconco for the Intelli-Sense Multi Speed Blower. This blower is meant for use with small labs that want a night set-back option for their fume hoods, and do not have the resources to sustain a VAV system.

So instead of going with rules of thumb, check out how laboratory equipment can work towards real energy efficiency.

Sometimes the latest equipment in a laboratory, say a next-generation sequencer, grabs lots of attention, but it’s the workhorses—centrifuges, hoods, freezers, incubators, and more—that keep experiments and workflows moving...

Read the entire article, Adding efficiency to general lab equipment by Mike May.

[1] Energy Use and Savings Potential for Laboratory Fume Hoods

 

Related Product Categories
Echo with model 2016

Filtered Fume Hoods

Fully-featured hoods that require no ducting use comprehensive filters to contain acids, bases and solvents. 

See Details

Ductless (Carbon-Filtered) Enclosures

Ductless (Carbon-Filtered) Enclosures

These enclosures use carbon filters and, in some cases HEPA filters, to protect users from exposure to hazardous fumes. No ducting is required.

See Details

Type C1 Axiom biosafety cabinet, class II biosafe cabinet

Biological Safety Cabinets & Enclosures

Class I and Class II biological safety cabinets are suitable for use with agents that require Biosafety Level 1, 2 or 3 containment.

See Details

Blowers

Remote Blowers & Exhausters

Remote blowers, designed for roof-mounting, provide airflow for fume hoods and other enclosures. Exhausters, designed for ductless applications, filter the air before returning it to the lab.

See Details