Search

4 questions to answer when selecting an evaporator

Tools for selecting laboratory equipment

You know that your process will require an evaporator, but how do you decide which one is right for your application? Answer these four questions to decide which evaporator would be the best choice:

1. How hot can my sample get?

“How much heat can be applied to my samples?” is one of the first questions you’ll need to answer.  In many methods, heat is the driving force of the evaporation process. Determining whether your sample is heat-sensitive or not will help narrow down which evaporation method is best for your specific scenario. Typically the evaporation process will involve a vacuum pump if a sample is heat sensitive, so the boiling point can be significantly lowered under the decreased pressure.

Evaporators for extremely heat sensitive samples                           

Evaporators for samples that can be heated-moderate or high

2. What is my sample volume?

The volume of your sample will be an important factor in determining the evaporator that will accommodate your requirements. Some evaporators can accommodate a wide range of sample sizes while others are designed for a very specific size of sample.

Evaporators for very large sample volumes > 250 ml

Evaporators for very small sample volumes < 1.0 ml

Evaporators that accommodate a wide range of sample volumes

3. How many samples am I going to evaporate?

The number of samples that you need to evaporate at one time will determine which evaporator is most appropriate for your application. Various types of equipment accommodate different numbers of samples.

Evaporator Type Maximum # of Samples
Rotary Evaporators 1 sample
CentriVap® Centrifugal Concentrator 132 samples  (1 to 2ml ea.)
FreeZone® Freeze Dryer/Lyophilizer  >2,000 samples
RapidVap® Vertex Dry Evaporator Up to 50 samples
RapidVap® Vacuum Dry Evaporator 110 samples (12 or 13mm tubes)
RapidVap® N2 and RapidVap® N2/48 Dry Evaporator Up to 48 samples (12 to 20mm tubes)

4. In what condition does the finished product need to be?

The condition or state of the final sample is a definite determinate of which evaporator is the best solution for your samples. Are your samples biological? Does their bioactivity need to be preserved for a long period of time? Does your method involve taking your sample to dryness, or do you need to stop the evaporation before the sample is dry? All of these factors need to be considered when selecting an evaporator.

Evaporators that preserve bioactivity and the final product can be a cake that is easy to reconstitute

Evaporators that can dramatically slow evaporation at specific end points

Evaporators with programmable time and heat temperature

 

Need help selecting the best evaporator for your samples?

 

 

TRY LAB EVAPORATION SCOUT

chevron_left Need Help Selecting a Concentrator? Articles How to select the right vacuum pump chevron_right