HomeLiteratureVideosFreeze Dry Systems

Videos for Freeze Dry Systems

Setting up a Labconco FreeZone Benchtop Freeze Dry System

Quick set up guide with instructions on connecting a FreeZone Benchtop Freeze Dry System to a vacuum pump and installing the chamber or manifold.

Programming the FreeZone Triad

Troubleshooting Vacuum Leaks in Labconco Lyophilizers

Learn to troublesoot vacuum leaks in Labconco FreeZone Freeze Dry Systems

Labconco Vacuum Pump Setup

Video describing the process of preparing a vacuum pump for installation and use with a Labconco FreeZone Freeze Dry System. Explains how to add oil, install exhaust filter, and more.

Preparing Pre-freeze Samples in Flasks for Lyophilization

Here are some simple tips to get the best results when freeze drying. These tips can also help you avoid breaking glassware, and help you select the best method of freeze dry preparation.

Programming the Labconco FreeZone Stoppering Tray Dryer

Setting up and programming the FreeZone Stoppering Tray Dryer to work with a FreeZone Freeze Dry System during lyophilization.

Setting Up the Labconco FreeZone Stoppering Tray Dryer

Video describing the process of setting up and installing a FreeZone Stoppering Tray Dryer for use with a FreeZone Freeze Dry Systems.

Aseptic Adapter Usage and Overview

Valved flask adapter to maintain aseptic conditions when freeze drying. Used with Labconco Fast Freeze Flasks 120mls up to 2000mls and Mini Stoppering Chamber. These adapters allow the user to fill a freeze dry flask under sterile conditions prior to lyophilization. After filling the flask, the valve is closed off isolating the contents for transportation to the freeze dryer. Once the flask is attached to the freeze dryer and a vacuum is pulled, open the flask to vacuum using the adapters valve. After freeze drying, close the valve and transport the samples back to the biosafety cabinet to open.

Freeze drying a cupcake: "Sublime at 40"

We freeze dried a cupcake in a Labconco FreeZone to celebrate the 40th birthday of Labconco Freeze Dryers. Come lyophilize with us!

Installing a large chamber on a small FreeZone Freeze Dry system

Labconco Freeze Dry History Trailer

40 years in 40 seconds: This short video trailer is compiled from highlights of the 5 minute history video wherein Executive Emeritus John McConnell describes the 40 year history of the Labconco Freeze Dryer from its development in 1972, to the first products in 1974, up to today (filmed in 2014).