HomeLiteratureVideosFreeze Dry System Parts & Accessories

Videos for Freeze Dry System Parts & Accessories

Troubleshooting Vacuum Leaks in Labconco Lyophilizers

Learn to troublesoot vacuum leaks in Labconco FreeZone Freeze Dry Systems

Preparing Pre-freeze Samples in Flasks for Lyophilization

Here are some simple tips to get the best results when freeze drying. These tips can also help you avoid breaking glassware, and help you select the best method of freeze dry preparation.

How To: Labconco Mini Stoppering Chamber setup and use

This video demonstrates how to set up and use the Labconco Mini Stoppering chamber to stopper small vials under vacuum. This Mini Stoppering Chamber can be used with FreeZone Freeze Dry Systems.

How to: Operating the Clear Stoppering Chamber

How to use the Labconco Clear Stoppering Chamber to stopper lyophilized sample vials under vacuum.

Aseptic Adapter Usage and Overview

Valved flask adapter to maintain aseptic conditions when freeze drying. Used with Labconco Fast Freeze Flasks 120mls up to 2000mls and Mini Stoppering Chamber. These adapters allow the user to fill a freeze dry flask under sterile conditions prior to lyophilization. After filling the flask, the valve is closed off isolating the contents for transportation to the freeze dryer. Once the flask is attached to the freeze dryer and a vacuum is pulled, open the flask to vacuum using the adapters valve. After freeze drying, close the valve and transport the samples back to the biosafety cabinet to open.

Freeze drying a cupcake: "Sublime at 40"

We freeze dried a cupcake in a Labconco FreeZone to celebrate the 40th birthday of Labconco Freeze Dryers. Come lyophilize with us!

Labconco Fast-Freeze Flask Adapters

Brief video detailing the installation of an adapter on a Labconco Fast-Freeze flask, as well as showing how tapered adapters can be reversed to accommodate both 1/2" and 3/4" flask tops.

Labconco Freeze Dry History Trailer

40 years in 40 seconds: This short video trailer is compiled from highlights of the 5 minute history video wherein Executive Emeritus John McConnell describes the 40 year history of the Labconco Freeze Dryer from its development in 1972, to the first products in 1974, up to today (filmed in 2014).