Search

Filtered Glove Boxes

These ventilated glove boxes feature inlet and outlet HEPA or ULPA filtration for particulate containment and user protection from hazardous materials.

Watch the Videos play_circle_filled
Filtered Glove Boxes
Protector Filtered Glove Boxes

These stainless steel or fiberglass-lined ventilated glove boxes feature inlet/outlet HEPA or ULPA filtration to protect the operator from hazardous materials.

Precise HEPA-Filtered Glove Boxes

These polyethylene-lined ventilated glove boxes feature inlet/outlet HEPA filters to protect the operator from hazardous materials.

XPert Weigh Box
XPert Weigh Boxes

These polyethylene-lined ventilated glove boxes feature HEPA filters, anti-static ionizer fan and a balance vibration isolator for weighing operations.

No Image
Protector Multi-Hazard Glove Boxes
These products have been discontinued

Find information on pre-2010 Protector Multi-Hazard Glove Boxes, which are now discontinued.

Labconco Filtered Glove Boxes feature HEPA or ULPA filtration and provide a leak-tight physical barrier to protect the operator from hazardous airborne particulates and powders. These boxes have uses in pharmaceutical research, nanotechnology and biochemistry. They are often referred to in the field as "Potent Compound Barrier Isolators" or "Hazardous Toxic Containment Isolators" in labs that produce pharmaceuticals.

Microorganisms, low-level radiochemicals, chemical carcinogens and asbestos may also be used in these boxes. These Glove Boxes may be used for cleanroom applications requiring ISO Class 3 conditions, and Labconco HEPA Filtered Glove Boxes may be appropriate for use as containment isolators for applications using compounds assigned ISO 4 and ISO 5 Banding Levels. Contact your Health and Safety Officer for specific Engineered Containment Device requirements.

Protector Filtered Glove Boxes

Video outlining the features and benefits of Labconco's Protector Filtered Glove Boxes. Protector Filtered Glove Boxes provide inlet and outlet HEPA or ULPA filtration and a leak-tight physical barrier to protect the operator from exposure to potentially hazardous materials.  These glove boxes feature particulate containment under 20 nanograms per cubic meter as confirmed by Safebridge Consultants, Incorporated and also meet ISO Class 3 standards.

Resources

lock Login or register to download resources

White Papers

Independent testing proves Labconco ULPA filtered glove box contains aerosolized nanomaterials effectively

by NanoSafe, Inc. on 2013-10-31

Labconco Corporation submitted its Protector® Stainless Steel ULPA Filtered Glove Box to an independent source to evaluate its ability to contain aerosolized nanomaterials...

View PDF (255.1 KB)



Recent Articles

Just How Precise is the Precise® Glove Box?

Labconco offers two rotational molded polyethylene-lined glove boxes with HEPA filtration: the Precise HEPA-Filtered Glove Box and the XPert® Weigh Box. Both of these boxes have a built-in blower and inlet/outlet HEPA filters to remove hazardous particulates...

Infographic: How to Select a Glove Box

Glove boxes provide a physical barrier to isolate sensitive materials inside from environmental contamination or to protect the operator from the hazardous materials being manipulated. Are you in the market? Here's what you need to know...

Independent testing proves Labconco glove box contains aerosolized nanomaterials effectively

Labconco Corporation submitted its Protector® Stainless Steel ULPA Filtered Glove Box to an independent source to evaluate its ability to contain aerosolized nanomaterials...

What to know about gloveboxes

The terms isolator, isolator glovebox, glovebox isolator, and barrier isolator are now commonly used to describe a glovebox and its functions. Unfortunately, expedient terminology usually falls short of defining the operational requirements for any specific glovebox. In general terms, there are two types of gloveboxes...